RELEASE NOTES
PowerAlert Device Manager 15.5.6 (Build 2002)
21-AUG-2019

Copyright (c) 2019 by Tripp Lite
All Rights Reserved

IMPORTANT NOTES
* Please be informed that in future firmware releases  beyond 15.5.x  the menu interface of LX Platform devices will
  no longer be supported. It will be replaced by a full-featured Command Line Interface (CLI), capable of the same
  functionality as the web interface.

REQUIREMENTS
* PowerAlert Mass Updater Utility version 1.1.0 (Build 17134) or higher can be used to upgrade
  prior versions of 15.x to 15.5.6.

DEFECT FIXES
* Stability and performance improvements

ENHANCEMENTS

KNOWN ISSUES
* Shutdown Device is written twice to the event log
* tlpEnvOutputContactCurrentState is not writable
* Device ID is not editable on 5009 and 5022 protocols
* An apostrophe character used when naming an action is rejected and causes consoles to log out
* Power On Delay always displays as zero for 5017 protocol
* Low and High Transfer Bounds are reported incorrectly for 5017 protocol
* Shutdown Device schedule does not work for 3005 protocol
* Low Transfer Voltage and High Transfer Voltage are reported in the wrong magnitude via SNMP for 5017 protocol
* Output Line Count is not displayed for certain devices
* Number of Phases is not displayed for certain devices
* Incorrectly displaying Enable Online Mode for certain devices
* upsSecondsOnBattery not supported
* Saving an auto probe via Menu interface will display an error when no IP address is specified on a disabled probe
* Clearing the default auto probes does not reset all changed fields to original values
* Modifying delay for the default email action may disassociate that action from events
* SNMPv2c not supported for Set OID actions
* Serial numbers are not editable using SNMP for devices that do not support serial numbers
* The web interface automatically logs out after a period of inactivity when the timeout period is disabled
* A space character is rejected when used for naming a device
* A space character used when entering a date is rejected and causes consoles to log out
* Incorrectly displaying Device Shutdown action when not supported by a device
* Incorrectly displaying Output Off event when not supported by a device
* Entering a session or inactivity timeout greater than 32767 locks Administrator out of web GUI sessions
* Configuring ACL for non-SNMP users is rejected
* sysContact is not configurable
* BMS serial number is not reported via SNMP for 3018 protocol
* System allows user to send multiple turn load on and off commands in a row
* System does not obtain an IP address from DHCP if network is not available during bootup
* Fan Always On and Remote Setpoint do not return to original value after dehumidifying event
* Fan Always On can be set after Remote Setpoint is disabled
* Reboot device will not operate properly if restart time is less than shutdown time
* "Save and Reboot" after changing a subnet mask sometimes does not save the change [Use save without reboot, then reboot the card instead]
* Changing a subnet mask to a value not in conformance with one's network will prevent all remote access to the system
* tlpCoolingQuietMode is listed in MIB as read-write, but should be read-only
* tlpCoolingHotGasBypass is listed in MIB as read-write, but should be read-only
* Hovering the mouse over role, keyword and importance in Device Settings displays incorrect values
* Lowest temperature setting (63 degrees) does not save for 9002 protocol
* Battery Age on 4006 protocol does not update and remains zero when Last Battery Replace Date exceeds 36 months
* Device Mode on 4006 protocol does not show Standby after placing the unit in Standby mode
* Reset Battery Transition Count should be listed as a Reset Control
* Water Full/Not Full messages appear during power cycles on 9002 protocol
* Operating Mode displays Not Connected when the LX card is disconnected on a 9002 Protocol [Reboot unit to correct]
* Load importance selector allows for choose values out of range (should be 1-100)
* Incorrect Nominal Output Voltage selections are presented on a 4201 protocol
* Nominal Output Voltage cannot be configured on a 4201 protocol
* Enable Online Mode should be listed as an Enable Control
* Auto Fan Speed does not automatically update on the GUI panel using IE (Updates are correct using Chrome and Firefox)
* Device ID reverts back to zero(0) regardless of value saved on SM8896 on 3021 protocol
* Battery Minutes Remaining does not display a value when on battery on PS6794 on 4100 protocol
* Battery Age Above Threshold alarm does not clear after changing replacement dates on PS6794 on 4100 protocol
* General Fault alarm does not trigger on PS6794 on 4100 protocol
* Output Off alarm does not trigger on PS6794 on 4100 protocol
* Output Calculated Power (KW) reports inaccurate value on PD88BF on 5013 protocol
* tlpPduOutletGroupIndex reports incorrect index value
* Device ID is not editable on 5009 protocol
* SNMP reports incorrect number of bypass lines supported by the 3-phases UPS on 4201 protocol
* Communications Lost category cannot be modified via Menu interface
* Unable to enable or disable bypass mode via SNMP
* SNMP reports battery voltage incorrectly on 4201 protocol
* Battery Warning value does not change when device enters Battery Low condition on 4201 protocol
* Output Power is reported twice on 4000 protocol
* Self Test Status does not update after executing self test on 4201 protocol
* Fan status not supported by UUT on 4000 protocol
* Output Source reports normal when main load is off on 3005 protocol
* Output Current Above/Below Threshold alarms are not cleared once the output current returns to normal on 5017 protocol
* Accounting logs have the same time stamp on multiple entries from different computers and usernames
* Nominal Input Frequency not reported via SNMP on 4000 protocol [Use GUI to view value]
* Phase Voltage Type, phase to phase or phase to neutral, not reported via SNMP [Use GUI to view value]
* Email log format setting reverts to XML after reboot
* Incorrect number of breakers reported on 5017 protocol
* Current tolerance not settable via SNMP [Use GUI instead]
* Cooling Compressor Status not reported via SNMP on 9003 protocol [Use GUI to view value]
* Turning all loads does not work on 3005 protocol
* Remote EnviroSense sensor not working correctly to set SRCOOL33K temperature
* Battery Low condition does not trigger when in alarm on 0003 and 0005 protocols
* tlpUpsEstimatedMinutesRemaining does not report data on 4004 protocol
* VA Rating reports incorrect value on 4008 protocol
* Alarm Status of "mute" does not reset to "enabled" when utility power is restored on 4007 protocol
* Bypass low limit cannot be changed via Menu interface on 4007 and 4008 protocols
* Battery Status only reports normal conditions on 4201 protocol
* Device Mode incorrectly reports shutdown condition as "other" on 4201 protocol
* Only two of a possible four error condition codes are reported via CLI on 4008 protocol
* Power On Delay cannot be reset back to zero on 4008 protocol
* Minimum Battery Restart value is out of range on 4007 and 4008 protocols
* Energy Saving value can be set to values out of range on 4007 and 4008 protocols
* Incorrect input values reported while on battery on 4005 protocol
* Reset Watt Hours not working on 4008 protocol
* tlpEnvOutputContactCurrentState does not change the state of the contact on 9300 protocol
* Cycling a load group does not clearly display state change between off and on
* Ramp and shed delays become out of sync when setting value via SNMP
  -- A 20 second idle timeout is invoked prior to writing ramp and shed changes to the device. All values set after
     the idle timeout expires are not written. Rebooting the device will reload the values from the device. An alternative
     is to use the GUI to set ramp and shed values.
* RTC is not set on 4009 protocol
* tlpDeviceIdentTotalUptime is missing UNITS (days) in the MIB
* Some smart battery packs are reported as non-smart on 4008 protocol
* tlpUpsConfigInputVoltage is returned in error when only output voltage is supported on 4006 protocol
* Bypass Limit values can be set outside of the operating range on 4007 and 4008 protocols.

END RELEASE NOTES